Why Isolation is Critical in an EV PTC Heating System
In an EV, the PTC heater runs off the high voltage battery to maximize the power delivered to the heater. An IGBT or other high current power device is used to turn the heater on and off, while voltage and current sensors monitor the input voltage and current draw. An MCU is used to manage the heater and communicate with the other systems in the vehicle. The diagram shown depicts a PTC heater configuration with the MCU in the low voltage domain.
Isolation is critical for enabling the MCU to monitor and control the PTC. An isolated IGBT gate driver, such as the Si828x, or FET drivers, such as the Si823x or Si8236, safely drives the main power device. The voltage and current measurements are made using isolated measurement devices such as Si892x. The entire system can be monitored and controlled via an automotive bus such as CAN or LIN which is isolated with digital isolators, including Si86xx and digital isolators with integrated dc-dc power converters such as Si88xx.